Part Number: TPS92602-Q1 Other Parts Discussed in Thread: TPS92602EVM Hi TI guys:
I am using the TPS92602-Q1 in my project, but there is a problem need your help.
when I turn on the VBAT1, the low beam work normally, then I change the power supply…
Hi Clint:
Thanks, for replying.
1. One LED is set at 27.5V. The subsequent current drawn is with in 430mA Nominal.
2. When the LED is strobed, it must stay on for about 100ms, although because this is a prototyping platform something that allows…
Hi Sakai-san,
Currently we don't have EVM based on flyback topology but it won't be difficult to modify one. All you need to do is to have a standard flyback board and we can connect control and feedback signals between TPS92602EVM and flyback board…