Part Number: TRF7960ATB Tool/software: Code Composer Studio Is there a library available for interfacing TRF7960ATB with MSP432P410R?
In case there is one, then do provide the link for it.
Part Number: TRF7960ATB Hi,
I want to use Direct Mode 0 with the TRF7960ATB board, I then need to access the IO_6 pin to demodulate the signal with a home-made circuit.
Is there a way to physically access this pin on the board ? I cannot open the .brd…
Part Number: TRF7960ATB Tool/software: Code Composer Studio Hello, where can I find the MSP-EXP430F5529 CCS C-Code project for the TRF7960ATB?
Regards,
MSP-EXP430F5
Part Number: TRF7960ATB Hello,
I need TRF7960ATB module base application firmware for MSP-EXP430F5529, but the link bellow is dead.
http://www.ti.com/lit/ug/slou372a/slou372a.pdf
8 Base Application Firmware -> MSP430F5529: http://www.ti.com/tool/n…
Part Number: TRF7960ATB Good morning,
I´m using the TRF7960ATB evaluation board whe I configure the ISO15693. I set the modulator and SYS_CLK control register (0x09) to 0x21.That means that the system output frequency should be 6.78MHz, because the bit…
Part Number: TRF7960ATB I have a TRF7060ATB and a MSP-EXP430FR5739 experimenter board with atb connected on two RF headers of the board, the launchpad is running but I couldnt find any reference/code to interface the two.
Can anyone help me get started…
Part Number: TRF7960ATB Sir or Madam,
I have established SPI communication with the TRF7960ATB and have been able to write and read registers using a proprietary SPI-USB device and custom software.
I have read the data sheet for the for the TRF7963A which…
Other Parts Discussed in Thread: CC2530 , RF430CL330H , TRF7960 , MSP430G2553 , TRF7970A , TRF7960A Hello all,
I am having some questions regarding using TRF7960ATB with ISO14443B at 106 kbps.
HW: TRF7960ATB rev B 2010 (according to silk screen) mounted on a…
Other Parts Discussed in Thread: TRF7960 , TRF7960A , TRF7970A Good morning,
I am using the evaluation board TRF7960ATB to apply it to my design. My goal is to communicate with the STM32F101RB MCU.
The problem is that I can not initialize the reader and I…