Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: TDA4VM
Hi, TI engineers,
We are trying to bring up the board with SoC TDA4VM SR1.1 HS-FS, We using HLOS SBL boot flow, but when running into the SBL, an error "TIFS load...FAILED" was occured.…
Hi Takuma,
Our target is to use display (DP0) under RTOS SDK environment (by vision apps). That means we need default R5F display. But it failed. So we tried using pure Linux SDK to test, it still failed. If you get confused, you can ignore the "Modify…
Part Number: J784S4XEVM We are working on a J784s4 dev board, running some benchmarks in QNX. We have been trying to configure MSMC as L3 Cache, and have been running into some issues. Some Background:
Board: J784s4 PDK 9.01.00.06 qnx710
Initially,…
Hi Kevin,
Since these are applications that have to tested independently, you could try the following methods to avoid conflict -
1. The /r5f_mpu_j784s4_default.c file present in PDK/packages/ti/drv/ipc/examples/common/src has the MPU region configurations…
Part Number: TDA4VM When running IPC communication based on Rpmsg on RTOS,Compile demo from TI :rtos-j721-evm-08_06_01_03/pdk_jacinto_08_06_01_03/package/ti/drv/ipc/example/common/src/ipc_testsetup.c
For example, Compile and run on mcu3_0,When using the…
Takuma Fujiwara said: One thing that I have found so far that I plan to look into is this E2E thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1311552/tda4vm-sdk-9-0-patch-for-edp-to-hdmi-bug/5035861#5035861
Actually, DP…
Oh,I'm blurred,as well as you can see below according to the TI instruction:
However, in "pdk_j721s2_08_06_01_03\packages\ti\drv\ipc"
or like this:
root@ubuntu:/home/django/TDA4VM_ECO/rtos_sdk_source/pdk_j721s2_08_06_01_03/packages/ti…
Hello Parth,
I was able to build the pdk library and create the example projects using the pdkProjectCreate.sh scripts. I had to modify the ccs version in the script.I have imported the project using CCS>File>Import>Code Composer Studio>CCS Projetcs and…
Hi,
Please follow these steps to boot to A72 Linux via SD card:
Generate lateapps by using the following commands
goto <RTOS SDK>/<PDK>/packages/ti/boot/sbl/example/boot_app/scripts
Run ./generate_lateapps.sh j721e_evm
Multicore…
Hi,
Sivaguru Subramanian said: 1. Does J721S2 has ethernet FW stack running on the R5F 2_0 (main domain).
No, Ethernet Firmware is supported only on CPSW5G & CPSW9G. J721S2 has CPSW2G instance, where EthFw is not supported.
Sivaguru Subramanian said…