Part Number: TSW38J84EVM Hello,
I'm using the TSW38J84EVM with the TSW14J56EVM to transmit BLE preambles by loading a csv into HS DC Pro, and upon reading the TSW38J84EVM output with an AD9082-FMCA-EBZ evaluation board, performing coarse frequency compensation…
Part Number: TSW38J84EVM We work with the TSW38J34 board. At the output of the modulator TRF3722 you can see the changes in signal amplitude. At the input of the modulator (I and Q) QPSK modulation signal. There is no amplitude distortion at the input…
Part Number: TSW38J84EVM I would like to use the FMC connector to provide SPI control of the TRF3722. The FMC connector has signals listed as FMC_B5 and FMC_B6, but there is no description of these signals that are provided to the CPLD on the TSW38J84EVM…
Part Number: TSW38J84EVM We are using the TSW38J84EVM module connected to a Xilinx Ultrascale+MPSOC Z102 and are intending to program the LMK04828 and the DAC38J84 through SPI signals that interface through the FMC connector and no program the SPI registers…
Part Number: TSW38J84EVM
When I set the PWR_TX_DIV to 0 (to enable the TX output) the board resets, requiring me to reconfigure the DAC, LMK and the TRF3722. I'm able to get the signal out of the DAC (measured on the current to voltage converter circuit…
Part Number: TSW38J84EVM Hi There,
I am working with the above development board. In the manual, it specifies that it accepts external power of 5v DC with the Barrel connector. it does not say whether the power supply should be "centre positve" or "centre…
Part Number: TSW38J84EVM Hi I have a query concerning the TSW38J84EVM board. Can the GUI be used to setup the board for demodulation? Or is this board just a modulator?
Part Number: TSW38J84EVM Hello all,
A professor ask,
" One of the student has a question in relation to interfacing with the TSW38J84EVM. We have a IQ Modulator implemented in Mathlab, but we now need to send data to the IQ Modulator Evaluation Board…
Part Number: TSW38J84EVM
Hi, I have a question relating to the SerDes lanes on the TSW38J84EVM board. Within the user manual under the basic test setup it says "On the Quick Start tab, setup the controls as shown in Figure 8. For the dual-channel DAC3XJ82…
Part Number: TSW38J84EVM Hi Support,
Referring to schematic (TSW38J84EVM-SCH_B.pdf) page 4. The Y1 122.88MHz component has 6 leads.
A look at BOM (TSW38J84EVM-BOM_B.xls), Y1 is Crystek CVHD-950-122.88.
A check on Crystek CVHD-950-122.88 datasheet ( http…