Part Number: UCD3138OL64EVM-031 Other Parts Discussed in Thread: UCD3138CC64EVM-030 , , UCD3138
Hello,
I am testing UCD3138PFCEVM-026 which is working as expected for single phase classic boost topology.
Now in first case, I used UCD3138CC64EVM-030 daughter…
Part Number: UCD3138OL64EVM-031 Other Parts Discussed in Thread: UCD3138
Hi,
I have a UCD3138OL64EVM-031 board with me.
I am trying to download available UCD3138 practice lab firmware codes (downloaded from: https://www.ti.com/tool/UCD-TRAINING-LABS ) …
Part Number: UCD3138OL64EVM-031 Hi,
I need your help on EVM bring up for UCD3138OL64EVM-031.
Here is my environment,
PC(Win10) - [USB Interface Adapter] - [UCD3138OL64EVM-031]
We can see usb adaptor and LED are on
Software : Fusion Digital Power Designer…
Part Number: UCD3138OL64EVM-031 Hi,
We tried to install FDPS but we are facing below error.
As for FDPS install, tried to update thru CCS but got below error.
HTTP Proxy Authentication Required: https://software-dl.ti.com/ccs/esd/CCSv11/Updates/content…
Part Number: UCD3138OL64EVM-031 Other Parts Discussed in Thread: UCD3138 ,
I am trying to get the UCD3138OL64EVM-031 kit working with Fusion Digital Power Studio. Upon establishing a connection with the UCD3138, if the Design tab is clicked, this fatal…
Part Number: UCD3138OL64EVM-031 Hi Sir:
we did some ADC test on UCD3138OL64EVM-031;
J12 was short and ad12s short, voltage on AD12 is around 0.4v by adjusting R17; ADC setting code like below;
void init_ADC(void) { AdcRegs.ADCCTRL.bit.MAX_CONV = 1; AdcRegs…
Part Number: UCD3138OL64EVM-031 Hello Team,
The user guide of the EVM states that Operating System requirements should be Microsoft Windows XP (32-bit), or Vista (32-bit), or Windows 7 (32-bit). Can you confirm this will not work on windows 10 (64-bit)…
Hello David,
We do not offer a feature like that in CCS. You will need a hardware EVM such as a UCD3138 open loop EVM ( https://www.ti.com/tool/UCD3138OL64EVM-031 ) to view the register map in the Fusion GUI.
Regards,
Jonathan Wong
Part Number: UCD3138ALLCEVM150 Other Parts Discussed in Thread: UCD3138A Hi,
I have a UCD3138OL64EVM-031 control board and I am working towards development of firmware for LLC converter prototype.
I request design Schematic and PCB files for UCD3138ALL…
Part Number: UCD3138A Other Parts Discussed in Thread: UCD3138OL64EVM-031 Hi,
When AD0 is used for the address pin sampling, the corresponding AD sampling value is higher than the theoretical value. After checked the waveform that the AD0 pin voltage value…