Part Number: UCD3138CC64EVM-030 Other Parts Discussed in Thread: USB-TO-GPIO2 Hi Texas Instruments Team,
Please let me know on the following
Which USB to GPIO adaptor is suitable with this EVM?
What is equivalent mating connectors for the 40 pin female…
hou.j
I am not sure what the issue might be, but here are some things to look into:
1) Is the ground of the computer and the ground of the board under test connected and at the same ground?
2) Is the 3.3V power supply for the pull-ups also connected…
Hi Anne,
Thanks for the response. I've updated my settings to include a 2.2K pull up, and updated the scanning options as you have specified. How can I proceed to configure/read/write the GPIO's? Is there any literature on this?
Thanks,
Mat…
Part Number: TMS320F28335 Hi Sir,
I had placed an ePWM module into the Simulink and set some parameters.
(I guess C2833x is for TMS320F28335, am I correct ?)
now I want to set the ePWM output to a GPIO pin, but under "Hardware setting" -> "Hardware…
If USB is always available, then yes I guess it can be connect high all time. Or possible driven using GPIO from HOST when USB enumeration is ready to proceed.
Other Parts Discussed in Thread: UCD9090 , USB-TO-GPIO2 I have a pb with TI Dongle 2022 ,USB to GPIO2 wich doesn't accept command lines like the old one TI Dongle 2006 ,USB to GPIO.
so it gives errors like :
exapmle:
C:\Program Files (x86)\Texas Instruments…
Part Number: MSPM0L1105 Dear Ti team,
How to control GPIO by API?
What I think is
DL_GPIO_setPins(GPIO_PWR_PORT, GPIO_PWR_P2_PWR_OFF_PIN) is set to 1
DL_GPIO_clearPins (GPIO_PWR_PORT, GPIO_PWR_P2_PWR_OFF_PIN) is set to 0
I use DL_GPIO_readPins(GPIO_PWR_PORT…
Part Number: BQ76925EVM Other Parts Discussed in Thread: BQ76925 , Hi Team,
I try to use USB-TO-GPIO to connect BQ76925EVM. When the bq76925 Evaluation GUI is lauched, the below fault is reported. The USB-TO-GPIO firmware is too old to support.
Where to …