I checked the MOD file and the model is present. Did you create a "Simulation Profile" and add the LIB file to it? That is how the simulator knows where to look for the model. From your message it seems like you have not done this and hence the simulator…
Please start the simulation with a resistive load so it can go though startup. When it reaches steady state, then you can switch on the current pulse to apply the transient.
What you are currently doing is drawing 3A current when Vout is 0V, whcih…
If you see the error message at the bottom, it looks like you are using an evaluation version. The models we provide will not run in an evaluation version. You will need a paid version of PSpice from Cadence to run this model.
Vlad,
I am able to reproduce your error. Evidently, it comes due to the fact that there is no probe on your schematic. Once you add a probe, it should work. Let me know if this resolves your issue.
Chuck,
The encrypted model will work in PSpice if you have that simulator. We are unable to release the unencrypted model publicly on the website for some devices in order to protect the IP. If you need the unencrypted model for this device, you can…
You don't have to name it. When you instantiate the GND pin, just leave it as the default. Where ever you are using GND (any kind) on your schematic, just use this default GND symbol (without making any changes)
Hi Will,
Please refer to the following FAQ for more information about encryption: There is already an option to export the design and model from WEBENCH to TINA-TI. Why not use that option?
You can not use a voltage source for this in a simulator (voltage across a voltage source is always fixed). Use a large capacitor with an initial voltage as a surrogate for the battery. Then you can see the discharge characteristics. The value of the…