Other Parts Discussed in Thread: TIDA-00302
Hello,
TIDA-00302EVM has an external protection circuit to support IEC61000-4-5 and IEC61000-4-4 tests.
The target of the document linked below is INA210-215, but is it also effective as a reference circuit for INA186?
Please tell me if it is sufficient as a protection circuit for testing IEC61000-4-5 and IEC61000-4-4 when it is replaced with INA186.
(The absolute maximum rating of VIN + and VIN- of INA186 is (GND-0.3) V (min) 42V (max))
・TIDA-00302
www.ti.com/.../tidu473.pdf
Best regards,
DDdoor