This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA186: an external protection circuit

Part Number: INA186
Other Parts Discussed in Thread: TIDA-00302

Hello,

TIDA-00302EVM has an external protection circuit to support IEC61000-4-5 and IEC61000-4-4 tests.
The target of the document linked below is INA210-215, but is it also effective as a reference circuit for INA186?
Please tell me if it is sufficient as a protection circuit for testing IEC61000-4-5 and IEC61000-4-4 when it is replaced with INA186.

(The absolute maximum rating of VIN + and VIN- of INA186 is (GND-0.3) V (min) 42V (max))

・TIDA-00302
www.ti.com/.../tidu473.pdf

Best regards,
DDdoor