This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV6001: Can someone suggest a substitute in a bigger package (easier to solder)?

Part Number: TLV6001
Other Parts Discussed in Thread: OPA348, TLV6002, TLV9002

I am using the TLV6001 as the differential to single-ended output stage of an isolated voltage sensing circuit, which is copied from SLAU733 (see attached). It's not high bandwidth and the voltages are constrained by the isolator to be under 4v. The supply to the opamp is 5v.

My problem is this - the TLV6001 is the hardest part on the board to solder because it is only available in SOT23-5 and SC70 packages. This product is a piece of test equipment, very small volume, and the boards are soldered by hand.

I'm not experienced enough to know how to substitute this opamp, but I'd like to find a part in an SO-8 or larger package that I could use instead.

Does anyone have any suggestions?

Thanks,

Lloyd