Part Number: INA592
Other Parts Discussed in Thread: INA818
Hi expert,
From below figure, the max common mode input high of INA592 is 54V:

However, from datasheet, the max input voltage is 3V+.

So I'm a little confused, if I use single supply V+=24V, V-=GND, what' the max input voltage? Should it be 54V or 72V?
Looking forward to your reply. Thanks.
Jiandong