This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA857-DIE: Transimpedance amplifier

Part Number: OPA857-DIE
Other Parts Discussed in Thread: OPA857, , OPA855, LMH32401, OPA858, OPA859, OPA856

Hello,

I was wondering if there are any experimental/test data about this device?

I would expect the input capacitance to be affected by the packaging of the OPA857, therefore I would expect a lower capacity and broader bandwidth for the OPA857-DIE compared to the OPA857.

And also as a consequence, if it's been tested with lower photodiode capacitance than 1.5pF. This is because the photodiodes I intend to use will have a capacitance of 0.3pF.

Kind regards,

Francesco