Other Parts Discussed in Thread: LM741, TL1431, OPA227, OPA197
I am using an OPA228 as a comparator. I use 1 OPA228 with a bias voltage of +15V on the +V pin and grounding the -V pin. I use a second OPA228 with a bias voltage of -15V on the -V pin and ground the +V pin. Each sub circuit compares and outputs a positive or a negative voltage with a singe bias supply. This gives me an easy way to compare voltage level from an AC input voltage. The simulation model seems to work fine. I remember LM741 opamps could run off a single positive or negative bias voltage which was great for making positive and negative voltage regulators.
Can I bias the OPA228 to operate in the manner above? Please advise.
Does the low voltage drift of the OPA228 make it a good candidate for a wide temperature range comparator using a TL1431 voltage reference?
Thanks
Jim