Part Number: TL061
Other Parts Discussed in Thread: TLC271
Dear Specialists,
My customer'd like to know the difference between TL061C and TL061I.
I would be grateful if you could advise.
---
Currently, we are using TL061CPSR (SO package), but it is a commercial product and there is no temperature regulation, so it seems to be a problem.
SO package is supported only commercial grade, it needs to investigate,
Could you please let us know following questions.
(1) Regarding the offset voltage, the MAX value of the TL061I is better than that of the TL061C, even though the temperature range is wider.
Are the dies inside using the same one or different one?
(2) TL061C is characterized at 0 to 70 ° C, is there any measurement data below 0 ° C?
---
I appreciate your great help in advance.
Best regards,
Shinichi