This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA192: Supply current

Part Number: OPA192

Hi,

1. Kindly let me know the Value of maximum current consumption of OPA192 @VCC=3.3V and VSS=-3.3V. 

2. I want to generate -3.3V from 5V supply. so how much output current i need to consider?

3. Aslo suggest me any IC having 5 to -3.3V suitable for OPA192.

4. Iam using Rsense =10R for high and low side sense(120ma and 24mA). Am i able to sense voltage by using this resistor?

5. Iam sensing 5mV also by using this opamp(gain maximum i can set is 1.8)Is it possible to sense?

Thanks 

Monisha OM