Other Parts Discussed in Thread: DRV8313
Hi there,
BACKGROUND:
I am having some trouble with the INA185 sensor that I use to sense the currents through a PMSM phases (phase A, B and C) as well as to sense the dc bus voltage. I have configured the sensors with a reference voltage Vref of 1.65V and VS of 3.3V and they are placed in a low-side topology (see top figure). Along with sensors, I use a DRV8313 that manages the PWM switching (see bottom figure). In a previous post (link) we discussed the need for a bidirectional sensor. Vm and the currents are quite low (Vm = 9V and currents is below 300mA) on a quite small motor wye-wound PMSM .


PROBLEM:
When I PWM the motor with a fix frequency with a duty cycle of 50% on phase B and phase C and 10% on phase A (just to test) I can measure positive currents through the motor. However, when I instead, on phase A, apply a duty cycle above 50%, the INA185 will not output anything lower than 1.544.
WHAT I HAVE TESTED:
I have checked that the motor does in fact experience a negative current in the oscilloscope by measuring the current through the DRVs output to the motor. I have also tested with various switching frequencies on the PWMs (2kHz to 10kHz). The lowside topo
Do You have any ideas on what the reason behind this problem?
Best regards,
Carl