Other Parts Discussed in Thread: BUF634
Hi,
section 8.3.3 of the BUF634A datasheet describes ESD protection feature and provides the following schematics. It's said that "current limiting resistors must be added at the inputs if common-mode voltages higher than the supply voltages are possible". RIN is a current limiting resistor foor VIN in the schematic.
It's also said, that protection diodes can typically support 10mA continuous currents. Does it also apply to the output Vo? How can I protect the oputput from overvoltage in an application where low-output-impedance is required (i.e. current limiting resistor can't be used)?