Part Number: INA592
Other Parts Discussed in Thread: INA149
Hello Guys,
Good day.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA592
Other Parts Discussed in Thread: INA149
Hello Guys,
Good day.
Our customer is using this component (INA592IDGKR) to record cell voltage data from a stacked battery system. The one drawback this has is they also need to stack the Vcc voltages, which can mean large supply voltages depending on the configuration.
Does TI have a newer version or any diff amps that don't need their Vcc voltages stacked to do this type of monitoring?
Thanks and regards,
Art
Hi Art,
Thanks for your post, I can help you.
What is the battery stack cell voltage? How many cells are there? Something like the INA149 could be useful since the input resistors are so large and can divide down the input voltage to a linear range.
Hello Tamara,
See below response from customer in verbatim.
"The total Stack voltage is 24V, 6S pack. I'd like to run the INAs from a separate voltage source.
There is a note in the datasheet that that family of opamps can have their inputs be a higher voltage than Vcc, since they are differential inputs. How much higher? could I have them monitoring a stack of 24Vdc while powering them from a separate 5V source?"
Thanks and regards,
Art
Hi Art,
the interesting question is how precise this voltage measuring shall be performed. Otherwise a simple OPAmp with a simple voltage divider can do the trick.
Kai
Thanks Guys.
I will ask customer about the precision of the voltage measurement and will update you guys.
According to the customer the image below from INA149 looks like what he is trying to do but this diagram does not mention the Vcc range needed. Does it have to be larger than the cell stack-up voltage?
Thanks and regards,
Art