Other Parts Discussed in Thread: TPS61094
Hi, this is the first time I have to solve this type of issue os summing 3 independent voltages with the common ground before an LDO. I'm trying to add 3 voltages, each one with a different buck-down regulator with Iout of <500mA.
That is, I have 1.2V, 1.8V, and 2.7V and at the final circuit I need 3.3V, normally I will use a Step Up Regulator on the 2.7V rail, but since the 3.3V are needed with at least 500mA using one voltage is not an option. Since the design is for an external board to these voltages, moving anything on the supply board is not an option.
That lead me to add the voltages, on an ideal op-amp works as expected, but when I'm trying to simulate it with the LM358B crazy values are obtained. So I have two questions.
a) Is the correct approach to use an op-amp to add the voltages?
b) How can I get correct results on the simmulation?