This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6521: Using dual LMH6521 in signal path

Part Number: LMH6521
Other Parts Discussed in Thread: LMH6629, LMH6517, LMH6518

Hello,

I would like some feedback in order to choose the best signal path for the following:

Input signal is single-ended 5-100MHz, with amplitude ranging over 300uVpp and 300mVpp.

I want to drive a differential ADC 2Vpp.

Noise performance is most critical issue here.

I had thought of using the LMH6629 in a gain of around 20 followed by both halves of the dual LMH6521 in series.

Using dual VGA will give me a variable gain over the 60dB that I need, and using a low noise gain block prior to VGA should render the noise of the VGA less significant.

 

In addition, are there any recommendations for driving LMH6521 by single-ended signal?

Thank you.