Other Parts Discussed in Thread: LM7705, TLV9001
Hi,
The customer configured the inverted OPAMP (Gain = -1) under the conditions of 5V Single supply, negative voltage input = -2.5V to 0V.

If I design it, I will use dual power supplies, but if the inverting AMP has a negative input as in the customer's design, is it okay to use a single power supply because the output is a positive voltage?
Also, if the input voltage can be less than -0.5V, it will exceed the absolute maximum rating. Is this okay if the input current is within 10mA?
The absolute maximum rating of the input current is 10mA.
I think this is the rated current of the ESD diode.
Best regards,
Hiroshi