Part Number: OPA2192-Q1
Hi team,
Do we have P2P device of OPA2192-Q1, but has higher voltage rating?(V+=36V, V-=-9V)
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2192-Q1
Hi team,
Do we have P2P device of OPA2192-Q1, but has higher voltage rating?(V+=36V, V-=-9V)
Roy
Hi Roy,
these are the OPAmps which can handle more than 36V supply voltage:
Kai
Hi Roy,
We have a few high voltage power amps that you may look at: https://www.ti.com/amplifier-circuit/op-amps/products.html#p1261max=45;180
Hi All,
Thanks for suggestion. But we need dual power input that could support V+=36V and V-=-.9V.
it looks that our solution couldn't meet the requirement.
Roy
Hi Roy,
this
V-=-.9V.
or this
V-=-9V
If the first is true, then just decrease the positive supply voltage a bit and use input voltage dividers, if necessary.
Kai
Hi Roy,
We do not have an exact high-voltage P2P replacement op amp that can drop into the OPA2192-Q1 board position. Links to high-voltage op amp alternatives have been suggested by Kai and Tamara, but these op amps will differ in their electrical performances from the OPA2192-Q1. Additionally, most of the high-voltage op amps have a enable/shut down function which require their EDCOM pin (pin 8) and a bottom side power pad be connected to certain voltages. Therefore, these high-voltage op amps would likely require PC board changes. And there is the Q1 requirement. When I check TI.com I don't see any of these high-voltage op amps available with the -Q1 extension.
It doesn't appear that we have a solution that readily works.
Regards, Thomas
Precision Amplifiers Applications Engineering