Other Parts Discussed in Thread: OPA1678,
The part is *not* listed as a rail-to-rail input and the stated input common mode voltage range is listed as extending to (V+) - 2V in section 6.7. Electrical Specs.
However, the block diagram shows a complementary input stage. Also the plots of offset and input bias current vs common mode voltage extend all the way to the positive supply. So judging on the available info in the datasheet, it pretty much is a rail-to-rail input. The spice model, too, seems to work up until the positive supply on the input.
What is wrong then ? The input common mode voltage range under 6.7. or all of the subsequent plots ?
Thank you very much.