Other Parts Discussed in Thread: TLV9054, TLV9064, OPA4322
Hi sir,
Could you pls kinldy suggest if there is P-P solution to replace ST TSV994AIDT ?
Thanks a lot!
(Wide BW 20MHz, R-R, 5V, CMOS OPA, small offset, quad)
Thanks a lot!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sean,
Does the application require the full 20MHz GBW or the 10V/us slew rate of the TSV994AIDT?
If these parameters can be reduced, a P2P solution can be proposed. Included below is a comparison table highlighting the performance differences between the TLV9054, the TSV994, and the TLV9064. The TLV9054 is a close match to the TSV994 in most characteristics, with the GBW being notably less. The TLV9064 has 10MHz GBW, with a 6.5V/us slew rate compared to the 10V/us of the TSV994.

I am happy to review the application to better understand any device specifications which are required.
Let me know if you have any questions,
Thank you,
Jacob