Using TLV9004IRTER with +/-3V3 rails. It is a low power application and unlikely to have thermal constraints with the thermal pad unconnected. Will the device will operate with bipolar rails without the thermal pad being connected if there are no effective thermal constraints? Appreciate that thermal pad connected to V- is recommended, and can sort on re-track. Just need guidance for prototypes which do not have the pad.....