Hello:
I am using the OPA211 low noise op amp in a low noise system where I need to use the shutdown option. I have two questions:
1. The datasheet reports that in shutdown the output assumes a high impedance state. However, since shutdown current is limited to 20uA, it appears that the input op amp stage is also shut down or partially shut down. So, in shutdown, can voltages within the rails be applied to the op amp inputs without those inputs drawing current beyond the normally tiny input bias currents? I have some high impedance nodes applied to the inputs that I need to not affect or pull around by the OPA211 being taken in and out of shutdown.
2. I could check this myself if there was a TINA TI op amp model for the OPA211 options (the DFN-8 and MSOP-8 package forms) that have shutdown. But, in the TINA TI "SPICE Macros => Op Amps" listing there are no versions of the OPA211. Nor do I find any TINA downloadable models on the TI website, though there is mention of PSPICE models. Is there a TINA TI SPICE model of the OPA211 with shutdown, or does that have to be simulated in PSPICE?
Thanks,
Farron