This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA-TI: TINA-TI series RLC circuit output at resonance

Part Number: TINA-TI

Trying to simulate RLC circuit in resonance with R=1ohm, L=1uH and C=138pF at 100mV @13.48MHz to 13.6MHz input. In AC analysis 38dB gain is showing at resonance but its not matching with multimeter or transient analysis data. In multimeter mode of Tina its showing 6V while in transient analysis its 4.66V. Why different values with different probing methods. Below is the snapshot of circuit and results.

Thanks in advance.