Other Parts Discussed in Thread: OPA820, OPA810, MUX508, , OPA1644, OPA4141, OPA2145
Hi,
I'm asking myself if there are J-FETs in the Input stage (for true MUX Friendly operation) or MOS transistors with some kind of gate protection clamping circuit like OPA820 ?
What happens with the + and - Inputs with very fast slewing input signal (Faster than the amplifiers slewing capability e.g. 200V/us) ?. Will there be a dynamic input current (beyond capacitive gate charge) like in the OPA820 or will it behave rather like a traditional J-FET amp and behave mainly capacitive ?
What is the maximum static (DC) differential input voltage, before typical Input bias currents exceed 1nA ?
Another quesion is about the availability of the new SOT-23-THN (DYY) package option. When will it be available ?
Thank you !