Other Parts Discussed in Thread: OPA4277, OPA277
Hello,
Is there are recommended configuration for 5962-16209 when a channel is not being used?
Thanks,
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Is there are recommended configuration for 5962-16209 when a channel is not being used?
Thanks,
Adam
Hi Adam,
The same rules will apply for this device as pretty much any other amplifier - it's best to place unused channels into a buffer configuration and buffer a voltage around midsupply. I would suggest a pair of 50k resistors to create the divider, in order to minimize the wasted current, and a 100 ohm feedback, to add a little phase margin. The feedback and input divider resistances should protect the inputs/clamps in case of an SET. The aforementioned component values will give you about 47 degrees phase margin with 10pF parasitic capacitance.
If you change the values around just be sure to do a quick sanity check for stability, my first instinct was to use 100k divider resistors but that resulted in a marginally stable circuit. Same thing if you anticipate higher parasitic resistance, it's always good to double check!
Cheers,
Jon
Thanks Jon,
One additional question, can you provide any technology information regarding the OPA4277-SP? I.e. are these CMOS, Bipolar, Unipolar, etc.?
Thanks,
Adam
Hi Adam,
Unfortunately I don't have a ton of information about the device that I can share from a process/technology perspective. However, I do know that the OPA4277 is fabricated on a bipolar process, with a bipolar differential input pair that includes input bias current cancellation circuitry (source). Hope that helps!
Cheers,
Jon
Hi Adam,
as the OPA277 contains 1k resistors at the inputs, I would do it this way, if powered from a bipolar supply voltage:
and this way, if powered from a single supply voltage:
Kai