This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM393B: Strange waveform when LM393B powers up at 0- -30C

Part Number: LM393B
Other Parts Discussed in Thread: LM339, TLV4021, TLV7042, TLV7041, TLV7021, TLV7022, TLV7081, LM393LV, LM139

Hi,

My customer uses LM393B as voltage detection.

when there is input power and ambient temperature is at >0C, it works normally as below.

CH1: Vo

CH2: IN+

CH3: IN-

ch4: Vcc(VBUS)

when there is input power and ambient temperature is at 0 - -30C, LM393B works strangely as below.

Vo has strange pulse but IN+ is lower than IN-.

the schematic is as below.

from Datasheet, LM393B should work at >2V and -25C.

Can you help check what happen?

BR,

frank