Other Parts Discussed in Thread: TLV3701
Hi,
Differential input voltage VID is 7V as per datasheet and it is measured at IN+ w.r.t. IN-. Does that mean VIN+ must be higher than VIN- every time? Why VID is not specified as +7V? Can we apply -2.5V to In+ while +2.5V to In-? Differential voltage will be -5V in this case. VICR range is -3.75V to +3.5V. So both inputs are within VICR or is there any violation of VICR?
Thank you.
Regards,
Vishal