This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3201: Propagation delay is not matching with datasheet parameters.

Part Number: TLV3201

Hello,

The datasheet propagation delay parameter is not matching with the simulation for sine input.

The delay with the sine input is 996ns which is not matching with the datasheet.

I have checked the same simulation with PWM input and the results are matching with the datasheet parameters. Please provide the input parameters for the sine inputs and the reason why it is not matching.

Thanks and Regards

Ashish Nawani