This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA544: Prototype Tests Vs Simulation Results

Part Number: OPA544

Hi Raymond,

We have performed tests with the circuit recommended by you (attached with the component value changes) with the change of the L&C values.

  • L & C Values recommended: 10mH & 1uF
  • L & C Values used in the circuit: 1.8mH & 10uF

Test Results Summary:

  • At 5KHz the circuit seems to be working fine
  • At 100KHz, we are able to get 30mVp-p for a Vin ripple of 96mV. But when the input ripple amplitude is increased to 104mV the output ripple jumps to 110mV. Similar behavior observed at higher frequencies also.

But in simulation, the circuit seems to be working fine.

Pl suggest if tuning of the component values will help to get a stable performance.

Best Regards,

Pons

opa544_08202021.TSC