This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM48100QMHE/NOPB



Hi,

    Can you provide below requested details ? part number: LM48100QMHE/NOPB.

 

1.Need the actual current drawn IDD & PVDD pins ,when 8 ohm speaker load connected condition.

2.Need the actual current drawn  I2CVDD pin, when 8 ohm speaker load connected condition.

 

 Please do the needful as soon as possible.

 

Regards,

Moorthi sekar

  • Hi Moorthi,

    Unfortunately there is not much help we can provide for this old legacy devices. There is no evaluation board available for us to perform any test. We would not be able to provide a typical value as this would need test in different conditions and a number of units.

    If there is anything else we could help let us know.

    Best regards,
    -Ivan Salazar
    Applications Engineer