Other Parts Discussed in Thread: TINA-TI,
Dear Sir,
We are using OPA2325IDR in the signal condition circuit.
we are giving signal Input : 0 to 5 V DC and getting signal Output in between: 2.4 to 2.5 V DC, but the expected output should be : 0 to 3.3VDC.
Output is not reaching the maximum output voltage of 3.3 VDC in IC1?
IC2 is working perfectly alright and the schematic is the same.
I am very confused, how to resolve this issue.
Please verify and suggest a solution.
Regards
Murthy