Part Number: TLE2071
Hi team,
I got a question from customer.
TLE2701 debugging, input waveform, but no output waveform,power +12V, please help to see what is the problem,.



Thank you very much for your help.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLE2071
Hi team,
I got a question from customer.
TLE2701 debugging, input waveform, but no output waveform,power +12V, please help to see what is the problem,.



Thank you very much for your help.
Best regards,
Hi Zewei,
this circuit looks very very strange to me.
When powering the LF357 in single supply mode and connecting the +input to signal ground you heavily violate the common mode input voltage range of LF375, as you must stay 4V away from the supply rails.
And connecting a cap at the -input of LF357, or by other words providing AC coupling, even forces the potential of -input going below the negative supply voltage. By this you even risk the destruction of chip.
I don't think that this circuit is correct.
Kai
The input common mode can't be ground It should be a t least 4V. Do you want the gain to be 10,000 (1M/100)? If yes, why is the input so large? Connect IN+ to a higher voltage.
Hi Ron,
I guess the LF357 is wired as fast slewing comparator using a dummy gain of 10000. There are many legacy circuits arround using this "technique".
Kai
thank you !
Zewei,
Bring pin 3 up to 4V which is a valid input common mode voltage. Then the op amp will work.
An alternative is to use a different op amp that allows input voltage down to ground. If interested, provided the full TLE2071 part number so I can search correctly.