Other Parts Discussed in Thread: LM124, , LM7705
Hi Team,
My customer is designing a circuit in which single supply (only for +Vcc) is fed to LM124. In Pspice simulations they are getting desired results, however when tried to simulate in hardware, output is non-linear at near zero range, are there any practical constraints to operate LM124 with single supply near zero.
Further details of the circuit are as follows-
Vbias (or +Vcc) = 13.7V
-Vcc= 0V (grounded)
Input range = 26 to 40V
Corresponding output range required = 0V to 5V
In hardware the output for 26V to 27.5V input remained constant at 0.634V.
From the below e2e discussion I understood that LM124 has two sink drivers as can be seen in the datasheet device schematic. One supports near GND voltage but can only sink tens of microamps. The other is the PNP output transistor that can sink more but needs 1 diode voltage diode of headroom to run.
Could you please suggest a way to mitigate the offset issue which customer is facing now in LM124A design. Can please help suggesting changes in below schematic so that the sink that supports near GND only gets activated i.e. how to limit sink currents.
Thanks in advance for the support.
Regards, Shinu Mathew.