Hello team,
My customer is using TL074I with +-12V supply, but in the datasheet, there is only +-15V specs. Could you please provide the VICM(common mode voltage input range) VOS(Maximum peak output voltage swing) under +-12V supply?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
My customer is using TL074I with +-12V supply, but in the datasheet, there is only +-15V specs. Could you please provide the VICM(common mode voltage input range) VOS(Maximum peak output voltage swing) under +-12V supply?
Thanks.
Zach,
Kai is correct about bringing all the values 3V lower (closer to ground)
I also suggest using the TL074H in new projects. It is a modern redesign of the ancient TL074.
Zack, Kai,
Back when TL074 was created, JFET was the way to get low input current because CMOS op amps were not practical at that time.
CMOS has advanced a lot since then. TL074H is different than most other CMOS op amps because the NMOS on input stage is primary (not secondary to just cover the top end of VCM). TL074H doesn't have any PMOS directly on input. So for both TL074 I and H, common mode near V- is not permissible.
Parameters | TL074H | TL074I |
Number of channels(#) | 4 | 4 |
Total supply voltage (Max) | 40 | 30 |
Total supply voltage (Min) | 4.5 | 7 |
Rail-to-rail In to V+ | Always | Usually |
GBW(Typ)(MHz) | 5.25 | 3 |
Slewrate(Typ)(V/us) | 20 | 13 |
Vos(offsetvoltage@ 25C) (mV) | 4 | 6 |
Iqperchannel(Typ) | 0.94 | 1.40 |
Vn at 1kHz | 37 | 18 |
Operating temperature range | [-40C,125C] | [-40C, 85C] |
Offsetdrift (Typ) (uV/C) | 2 | 18 |
Features | EMI Hardened | |
Input bias current(Max) (pA) | 120 | 200 |
CMRR (Typ) (dB) | 105 | 100 |
Output current (Typ) (mA) | 26 | 10 |
Architecture | CMOS | JFET bipolar |