This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Choose a dual op amp with low offset voltage, small IB and small IQ suitable for smoke detectors.

Other Parts Discussed in Thread: OPA2344, TLV9002, TLV2432A, TLV2262A, TLV9102, OPA2990, TLV9062
could you help choose a dual op amp with low offset voltage, small IB and small IQ suitable for smoke detectors. Specific requirements are as follows:
  1. Dual op amp, SOIC8 package;
  2. RRIO;
  3. Voffset is less than 1mV, preferably less than 0.5V;
  4. IB is not more than 200pA, and it is better to be less than 50pA;
  5. The IQ of each channel does not 200μA;
  6. Support 3V single-ended power supply;
  7. The GBW is not less than 0.5MHz, and 1MHz or more is better.