Other Parts Discussed in Thread: TIDA-00313, INA238
Hi Sir,
My customer refer to the TIDA-00313 Basic Block Diagram to do the INA226 application circuits for voltage sense from -23V to +36V.
Could you please help to review the schematics is available or not?
Programmable power system_V1_0924.pdf
*The U702 is monitored the net-name "GNA_INA-7.7V" is equal the -7.7V or not.
And the net-name "VS_INA" is 4.7V.
*The voltage sense circuit from -23V to +36V.