This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903: During power-on, what is the output status

Part Number: LM2903
Other Parts Discussed in Thread: TL431, LM393LV

Dear Teams,

My customer is using LM2903. They are wondering what is the output status (H or L) during the power on? I do see that TLV704X has a POR circuit to determine the output status (H or L) during the power on. Thus, LM2903 output status will be floating because it does not have internal POR circuit, right? Also, if we add a pull-low resistor at the output end, then the output status will be L during the power on, am I right?

Thanks!

Dylan