I have imported the .lib into Altium to create the simulation but it does not seem to be working properly.
The Error i am getting is that the Op-Amp is outputting the VSS value and not the amplified input voltage (it doesn't seem to register the actual VSS value in the circuit), If I use an generic Op-Amp it works fine. Has any one else saw this issue before and would some type of solution to help with fixing the error?
Below is the screenshot of the parameter values and the subcircuit code.