We have 4-20mA pressure transducers with a typical XTR106 recommended board. If we put one transducer in the test stand, we get a nominal 4mA output at zero pressure. If we add a second transducer, the first one's output may go down or go up 40 to 80uA. The direction and magnitude are transducer dependent. Adding a third transducer usually increases the up/down shift. Why does adding a transducer change the output? We found this when using MCC USB-2416 DAQ, or just using two handheld DMMs. The plot below starts with 3 transducers in test, then one, then two, then three, and repeats the sequence starting with a different Serial Number.