Other Parts Discussed in Thread: TLV6001, AMC1300
Hello,
We have to worry about common mode voltage range down to 0V at the output. (The DAS input is +/- 10V, AC coupled, with 50 ohm isolation to ground and 10M between High and Low pseudodifferential input (NI-4497 through a 2144 breakout). As for the common-mode voltage, it would be ideal to bring that down to 0).
We realize we possibly need a second stage amp(see below) that takes the diff out put of the AMC1200 and converts it to single ended. This is what we are thinking presently, but want to check with TI to make sure we can still meet our CM requirements. Do you think this would work?
Thanks,
Adam