Other Parts Discussed in Thread: INA233
Hi team,
Customer planned to use INA233 but changed to INA236 due to some reason.
INA236 looks not to assert if the current exceeds expected max current, unlike INA233.
Is my understanding correct?
If so, shoud I set the limit of shunt voltage to realize asserting high when overcurrent?
It means register setting will be below if my expected max current is 5A and shunt resister is 10mohm, right?
Other registers are default value.
6h: 8000h (SOL is 1 to set shunt voltage limit and bit11-14 are 0)
7h: 4E20h (20000d = 5A*10mohm/2.5uV)
Best regards,
Koyo