Other Parts Discussed in Thread: LM393B
Hi Team,
The customer is asking that the maximum case temperature of LM393BIDGKR. I can only find the ambient temperature in the DS. Thank you.
Best regards,
Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Mike,
With low power, low self heating devices such as this, Ta is assumed to be Tj.
The maximum operating temperature is 125C, which would be ambient. The actual die temp is a degree or two higher due to power dissipation, but the extra die temperature is covered in the characterization.
What are they trying to calculate or estimate?
All the available thermal resistance values are in table 6.5.
See the Semiconductor and IC Package Thermal Metrics report for more information on the parameters:
Mike
we have not seen any new engagement on this post, so I will be closing it. If you need further support, feel free to reply or start a new post.
Thanks
Chuck
Hi Paul and Chuck,
Thank for the support, the customer just want to make sure the device can operate in 90 degreeC. It seems that it is workable.
Best regards,
Mike