Other Parts Discussed in Thread: TCA9800, INA226, ISO1541
Hi sir,
I am looking for a pin to pin compatible device of INA238, with 0.3V VIL instead f 0.4V
Or ant method to make INA238 work with around 0.9V VIL.
Don't have to be 0.3V of Vdd, the device will be used with I2C isolator, as long as the VIL is above 0.8V in 3.3V, it will be fine.
Or is there any method to increase VIL of INA238?
Thanks.
Regards,