Part Number: TLV2333
Other Parts Discussed in Thread: LMV358, OPA2365, , OPA2333
Hi team,
customer use tlv2333 in below circuit. when using tlv2333, output distorted as third picture. when using opa2365/lmv358, output is not distorted as second picture.
The input signal is 1kHz.
Power supply is 3.3V single supply.
I asked customer to lower the input frequency in case the distortion is caused by lower bandwidth, when input frequency down to 50Hz, output is not distorted.
But for 1kHz, 6.8 gain, 350kHz bandwidth seems ok. Could you pls advise on it? Thanks!