Other Parts Discussed in Thread: INA333
Hi team,
I found the statement below on the datasheet "Power Supply Recommendations". Which specification will be reduced by using power supply below 3.3V e.g. 2.2V?
I saw the input common-mode range and output voltage are depends on the supply voltage, but I want to know anything else.
"The minimum power supply voltage for INA317 is 1.8 V and the maximum power supply voltage is 5.5 V. For optimum performance, 3.3 V to 5 V is recommended."
Regards,
Kazuto