Good Morning,
I have a current sensor chip (ACHS-7123) which gives 0.5V at -30A, 2.5V at 0A and 4.5V at +30A.
I only have positive currents.
My ADC (ADS1015ID) has a range of 0-4V.
I want to build a level shifter to get ~0V for 0A and ~4V for 30A to use the ADC range as good as possible.
And some filtering of the signal is also a nice idea.
Here my solution:
I_Sensor Signal Conditioning.TSC0118.I_Sensor Signal Conditioning.TSC
It gives a nice result, but maybe there is a better solution out there.
And: I have to use this chips, cause the original design used them and we have a stock.
With best regards
Gerhard